Encyclopedia search

重新搜尋
顯示由 51 到 60 的 323 結果
Constant flow, control mode
Constant flow is used in systems where there is a demand for a constant flow independent of the pressure loss.
Constant pressure boosting
Increasing water pressure to a certain set point and keeping the pressure regardless of flow and inlet pressure.
Constant pressure, control mode
Constant pressure, control mode
Consumption profile
The consumption profile shows the relationship between the time of the day and the water flow rate.
Cooling ceiling
Water-carrying cooling ceilings can be used as a supplement, if cooled-air temperature regulation systems are insufficient.
Cooling jacket
A cooling jacket enables a portion of the pumped liquid or an external liquid to be circulated around the motor stator housing.
Cooling surface
A cooling surface is used for cooling of outside air before injection into the building.
Cooling tower
A cooling tower is used to remove excess heat from an air-conditioning system if the heat cannot be utilised for another purpose.
COP (Coefficient of performance)
Coefficient of performance (COP), is an expression of the efficiency of a heat pump.
Corrosion
Corrosion can occur on external and internal surfaces of pipes, tanks and radiators.